As nossas marcas

Bem-vindo ao website da Schneider Electric

Bem-vindo ao nosso site.
		
Como o podemos ajudar hoje?
In programming PID, what does parameter FbS do on an ATV312 drive?
Issue:
Parameter FbS (feedback scale factor)

Product Line:
ATV31 and ATV312

Environment:
All models and serial numbers

Cause:
None

Resolution:
The parameter FbS is a parameter that can be used to scale the reference according to the range of the feedback sensor.
Example: Regulating pressure
PI reference range of process, 0-50 psi (0-100%)
Range of pressure sensor, 0-100 psi
FbS = Max sensor range / Max process range
FbS = 100/50 = 2