As nossas marcas

Bem-vindo ao website da Schneider Electric

Bem-vindo ao nosso site.
		
Como o podemos ajudar hoje?
ATV61HC**N4 drive is found with control block VX4A61201Y(not commercialised). As per ATV61 spare list the reference is VX4A61101Y, Can we use VX4A61101Y?

The spare part  reference for ATV61 drive control board (drive upper to 75kW) is VX4A61101Y.
The second reference VX4A61201Y was released for testing and the same was cancelled.

The drive will work without any problem with control board reference VX4A61101Y, hence you can use the same to replace the control board.