As nossas marcas

Bem-vindo ao website da Schneider Electric

Bem-vindo ao nosso site.
		
Como o podemos ajudar hoje?
Maximum table in a recipeDB
Issue

While using the RecipeDB with the factorycast HMI, exceeding the maximum number of tables will cause the module to fail, this was tested with an automatic SQL request.

Product Line

Factory cast HMI (WMY, NMW)

Resolution

The maximum number of tables should be limited to 6 with 50 variables of 2 octets per table to insure a stable system.