As nossas marcas

Bem-vindo ao website da Schneider Electric

Bem-vindo ao nosso site.
		
Como o podemos ajudar hoje?
Are there different licenses for Vijeo Designer Runtime based on tag counts or number of tags used?
Issue:
Are there different licenses for Vijeo Designer Runtime based on tag counts or number of tags used?

Product Line:
Vijeo Designer Runtime Software
VJDSNRTMPC, VJDSNRTSPC

Environment:
HMI runtime software for Windows

Resolution:
Vijeo Designer Runtime is a single license that is not based on tag count or number of tags used.  The Runtime license is fully functional to all features in Vijeo Designer development as long as the hardware supports it.  The Vijeo Designer Runtime can run on the Harmony/Magelis Industrial PCs (iPCs) or a Standard Windows PC.

For Vijeo Designer v6.2 Service Pack 10 and older, the part numbers were (and are no longer commercialized):
VJDSNRTMPC Runtime iPC
VJDSNRTSPC Runtime Standard PC

For Vijeo Designer v6.2 Service Pack 11 and higher, the part numbers are:
VJDRPCCZLSPMZZ - Vijeo Designer Runtime, Standard PC & Harmony PC (except HMIBMP,HMIBMU,HMIPSO,HMIPSP,HMIPEP), printed
VJDRPCCZLSPAZZ - Vijeo Designer Runtime, Standard PC & Harmony PC (except HMIBMP,HMIBMU,HMIPSO,HMIPSP,HMIPEP), email
VJDHPCCZLSPMZZ - Vijeo Designer Runtime, Harmony PC ( HMIBMP,HMIBMU,HMIPSO,HMIPSP,HMIPEP)/Harmony P6, printed
VJDHPCCZLSPAZZ - Vijeo Designer Runtime, Harmony PC ( HMIBMP,HMIBMU,HMIPSO,HMIPSP,HMIPEP)/Harmony P6, email