Pesquisar nas perguntas frequentes (FAQ)
Which is the correct variable for MV presence which co-relates to pin no. 8 of Mate N-Lok 9 pin connector in T200S ?
1.1 - Question
Which is the correct variable for MV presence which co-relates to pin no. 8 of Mate N-Lok 9 pin connector in T200S ?1.2 - Application
This FAQ is applicable when it is required to identify correct variable for a digital input for MV presence.1.3 - Answer
The variable Aux._MV_Presence_x (TSS54 for switch-1 and TSS85 for switch-2) co-relates to pin no. 8 of Mate N-Lok 9 pin connector in T200S. These two are the only variable for voltage presence/absence, which will be used by Automatism function for switch-1 (TSS54) and switch-2(TSS85) in T200S.The variable MV_Presence_x (TSS73 and TSS105) are for T200P, where it will be derived from Voltage measurements.