As nossas marcas

Bem-vindo ao website da Schneider Electric

Bem-vindo ao nosso site.
		
Como o podemos ajudar hoje?
How do I change the direction of rotation on Lexium 32 ?

If you simply want to invert the direction of rotation when the motor makes motion you need to change the parameter called InvertDIrOfMove

The factory default value is set for Inversion Off.   In which case the motor shaft rotates clockwise for positive movements and counter clockwise for negative movements.

By changing this parameter to Inversion On the rotational direction of the motor will be inverted.  Thereby causing the motor shaft to rotate counter clockwise for positive movements and clockwise for negative movements.

The parameter InvertDirOfMove is accessible from SoMove and also via the built-in HMI.

In SoMove you will find this parameter in the section "Axis Configuration > Drive

Via the build in HMI you will find this parameter at "Conf > ACG > InNo

The parameter number is Modbus address 1560

Note that changing this parameter will require you to perform a drive restart  "cycle the power to the drive".



If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)