As nossas marcas

Bem-vindo ao website da Schneider Electric

Bem-vindo ao nosso site.
		
Como o podemos ajudar hoje?
Video: How to Find the CPU Load for an ION Meter

Issue
How to determine the CPU Load in an ION meter.

Product Line
ION7300 series
ION7400
ION7500
ION7550
ION7600
ION7650
ION8600
ION8650
ION9000
PM8000


Environment
ION Setup will be used to find the CPU load.

Cause
ION modules in the template consume CPU power.  In cases were it is desired to add custom frameworks, it is necessary to keep track of the processing power available.  Once the processing power reaches the limit of 100%, it would not be possible to add extra modules.

Resolution
While the following video below goes through the procedure, here are the steps:

  1. Using ION Setup connect to the meter (in this example single mode is used to connect to an Ethernet meter)
  2. Click on Exit to close 'Setup Assistant'.
  3. Select 'No' when prompted to connect to a different device to keep the connection open to the meter.
  4. From the menu, select Tools > Diagnostics.
  5. Select 'General' tab.
  6. Observe 'CPU Loading' parameter.