As nossas marcas

Bem-vindo ao website da Schneider Electric

Bem-vindo ao nosso site.
		
Como o podemos ajudar hoje?
What is the part number for ATV630 and ATV930 Extended I/O option card?
Issue:
ATV630 and ATV930 extended I/O option card part number.

Product Line:
ATV630, Altivar 630, ATV930, Altivar 930, Process Drive

Environment:
All

Cause:
NA

Resolution:
The part number for Digital and Analog I/O extension module is VW3A3203. The card expands the available I/O with an additional Six Logic Inputs, Two Logic Outputs, and Two Analog Inputs.