As nossas marcas

Bem-vindo ao website da Schneider Electric

Bem-vindo ao nosso site.
		
Como o podemos ajudar hoje?
What is the maximum current consumption on the internal +24vdc power supply on the ATV630 and ATV930 Process drives?
Issue:
Current consumption of the internal +24V DC power supply for the Altivar Process Drives ATV630/930

Product Line:
Altivar ATV630 and Altivar 930

Environment:
All

Cause:
Want to know if they can  use the drives built in +24vdc power supply to power up a PLC card.

Resolution:
24V Output power supply for digital inputs and safety
function STO inputs O =  +24 Vdc
 Tolerance: minimum 20.4 Vdc, maximum 27 Vdc
Current: maximum 200 mA for both 24 Vdc terminals
 Terminal protected against overload and short-circuit
 In Sink Ext position, this supply is powered by external PLC supply