Pesquisar nas perguntas frequentes (FAQ)
Osisense XC - UL or CSA certificate of the XCKJ10513C limit switch
The XCKJ10513C limit switch is produced in China (C at the end of the reference) for their market. It is neither UL, neither CSA, neither EAC approved or certified. Attached picture of the XCKJ10513C limit switch. Country of origin is China. On the front cover the CCC certification mark exists. The XCKJ10513(H29) limit switch reference is UL, CSA, EAC, CCC certified
Publicado para:Schneider Electric Portugal
Anexo(s)
Explorar mais
Explorar mais