As nossas marcas

Bem-vindo ao website da Schneider Electric

Bem-vindo ao nosso site.
		
Como o podemos ajudar hoje?
What would cause the ATV630 process drives fault relay not to change state after the external fault is activated?
Issue:
Cause of fault relay not changing state after the external fault is activated on the ATV630.

Product Line:
ATV630 and ATV930

Environment:
All

Cause:
The auto restart is preventing the relay from changing until the timeout is over.

Resolution:
The auto restart will prevent the fault relay from turning on until after the auto start time delay.