As nossas marcas

Bem-vindo ao website da Schneider Electric

Bem-vindo ao nosso site.
		
Como o podemos ajudar hoje?
ATV12 what would cause the drive to show ULF Underload Fault?
Issue:
Possible causes for ULF Underload Fault on ATV212 Drive.

Product Line:
Altivar ATV12

Environment:
All

Cause:
Programming

Resolution:
Under [ConF] > [FULL] > [I_0-] > [ULt] Underload monitoring was set to 3s.  If you do not want that monitored set back to 0s.