Como o podemos ajudar hoje?

Unity Pro V13.0 simulator goes to HALT.

On your PC is installed Unity Pro V13.0 and the Hot Fix UnityPro_V130_HF0435420R_Simulator_Windows10_v1709 installation.

On this PC when is openned an Unity Pro project done before this HF be installed and using the Unity Pro simulator then the simulator goes to HALT.

To solve this issue it is mandatory to do a Rebuild All of the Unity Pro application.