As nossas marcas

Bem-vindo ao website da Schneider Electric

Bem-vindo ao nosso site.
		
Como o podemos ajudar hoje?
What does the triangle LED on the ATV320 drives indicate?

Article available in these languages: Japonês

Issue:
ATV320 triangular LED indication

Product line:
Altivar Machine Altivar 320

Resolution:
When the triangle LED is on, the Drive is in a Fault condition. Check the display for the fault code to troubleshoot.
The LED goes off when the fault is cleared and the drive has been reset.

fault LED