As nossas marcas

Bem-vindo ao website da Schneider Electric

Bem-vindo ao nosso site.
		
Como o podemos ajudar hoje?
Where can I find the ground terminal on the High HP ATV630 drives?
Issue:
Connecting the power wiring and has a PE terminal, but there is not one marked with the ground symbol.

Product line:
Altivar 630, ATV630 Altivar Process

Environment:
Frame sizes 6, 7A, 7B

Cause:
Markings missing

Resolution:
Frame sizes 6, 7A and 7B have a power terminal marked PE for the ground.  The smaller Frame sizes just have a power terminal with a ground symbol.