As nossas marcas

Bem-vindo ao website da Schneider Electric

Bem-vindo ao nosso site.
		
Como o podemos ajudar hoje?
What terminal block is used with the BMXDAI1614 module?
Issue:
Selecting terminal block for the BMXDAI1614.

Product line:
x80 I/O

Cause:
Need part number for terminal block for the BMXDAI1614.


Resolution:
The terminal blocks for the module can be one of the following;
BMXFTB4000   caged terminal block
BMXFTB4020   spring terminal

Hardened version
BMXFTB4000H  caged terminal with gold plating
BMXFTB4020H  spring terminal block with gold plating