As nossas marcas

Bem-vindo ao website da Schneider Electric

Bem-vindo ao nosso site.
		
Como o podemos ajudar hoje?
Is it possible to downgrade M580 CPUs "new hardware" with old firmware (<V2.90)?
In  Jully 2019, we have published a new firmware SV2.90 for M580 PLC range. This new Firmware is required to manage a new embedded Switch (new hardware).
If you try to downgrade a M580 CPU (new hardware) with a firmware <V2.90, Unity loader will reject the downgrade.
New M580 CPU HW can’t be downgrade with old FW(<2.90) whatever the Unityloader version.