Pesquisar nas perguntas frequentes (FAQ)
Modicon M221 - TM3 bus doesn’t work with TM3DM24R or TM3XTYS4 SV 2.0
- Problem description:
If TM3DM24R or TM3XTYS4 module is placed before TM3 analog input modules (TM3A* or TM3T*) with TM221 controller.
- Results:
- The system word %SW118 is different than 16#FFFF (bit 13 or bit 14 is set to 0).
=> This issue is fixed by the M221 firmware version v1.10.1.3 attached to this FAQ.
- How to update M221 with .mfw file:
See attached document.
Publicado para:Schneider Electric Portugal
Anexo(s)
Explorar mais
Gama:
Explorar mais
Gama: