Como o podemos ajudar hoje?

what is electrical signal level expected by a BMXEAE0300 coupler to manage an Absolut coder (SSI compliant)?

The DATA0 + and DATA0- signals are symmetrical.
The DATA0 + involve from 0 to 3.5V and the DATA0- signal varies from 0 to -3.5V.
In differential, the DATA0 + and DATA0- signal varies from -3.5 to + 3.5V.