Pesquisar nas perguntas frequentes (FAQ)
Regarding RE17LMBM; What is its output state? Is it PNP or NPN output?
The RE17LMBM product uses thyristor device to perform switching. It relied on 24 to 240 Vac source to operate. This product is not suitable for DC load application.
Refer to attachment, the product’s wiring diagram for more detail information.
Refer to attachment, the product’s wiring diagram for more detail information.
Publicado para:Schneider Electric Portugal
Anexo(s)
Explorar mais
Produto:
Explorar mais
Produto: