Como o podemos ajudar hoje?

How can I enter into Resi9 MP with tubes without gland keeping IP?

Issue:
Keep IP protection when entering into the Resi9 MP enclosures with tubes without gland.

Product Line:
Resi9 MP

Environment:
Installation phase

Resolution:
You may enter into Resi9 MP surface with Tubes without gland thanks to easy removable entry cable you could adapt to cable section.

Notes:
To select the right enclosure, please select the product with the commercial reference starting with MIP10 / MIP11 / MIP 12.
Video - Resi9 MP - Entry Cable Management