Pesquisar nas perguntas frequentes (FAQ)
How to disable the system error popup window in Vijeo Designer?
Please refer to the setting in the following picture:
The setting gives you the option to turn system error window on or off.
Select Yes to show system error message window on the panel at runtime. If you select No, the panel will hide the window.
This property does not affect the generation or logging of system error messages, which can still be viewed using event summaries and the system error log viewer.