Pesquisar nas perguntas frequentes (FAQ)
Is a 4000A I-line distribution section available on a QED2 switchboard?
Issue:
Wants to have an I-line distribution section rated same as his 4000A main bus
Product Line:
QED2 switchboard
Environment:
All
Cause:
N/A
Resolution:
No, The maximum I-line interior made is 3000A and it is only available as single row. Double row interiors are 2000A max.
Publicado para:Schneider Electric Portugal
Explorar mais
Gama:
Explorar mais
Gama: