Pesquisar nas perguntas frequentes (FAQ)
Geo SCADA, x70 Controllers and Realflo compatibility
Realflo support for SCADAPack x70 controllers was first introduced in Geo SCADA 2020; offering support for flow computer 7.0
Realflo support for SCADAPack 47x controllers was first introduced in RemoteConnect 2.4.1 offering support for flow computer 7.01
Geo SCADA 2021 and Geo SCADA 2022 have support for later versions of Reafllo flow computer and x70 firmware versions.
This document aims to assist users in understanding which versions of Realflo flow computer and SCADAPack x70 firmware are supported by Geo SCADA and RemoteConnect.
Taken from 'What's New' in Geo SCADA Expert 2020 (ViewX Help)
Taken from 'Driver Reference | SCADAPack Modbus Realflo Driver | Introduction to the SCADAPack Modbus Realflo Driver' (ViewX Help)
Taken from 'Driver Reference | SCADAPack x70 Driver | Introduction to the SCADAPack x70 Driver' (ViewX Help)
In Geo SCADA 2021, support has been extended for x70 controllers runing flow computers 7.02
Taken from 'What's New' in Geo SCADA Expert 2021 (ViewX Help)
Taken from Driver Reference | SCADAPack Modus Realflo Driver | Introduction to the SCADAPack Modbus Reaflo Driver
Taken from Driver Reference | SCADAPack x70 Driver | Introduction to the SCADAPack x70 Driver
In Geo SCADA 2022, support has been extended for x70 controllers running flow computers 7.10.2
Taken from 'What's New' in Geo SCADA Expert 2022
Taken from Driver Reference | SCADAPack Modus Realflo Driver | Introduction to the SCADAPack Modbus Realflo Driver
Taken from Driver Reference | SCADAPack x70 Driver | Introduction to the SCADAPack x70 Driver
Summary of Realflo functionality added to RemoteConnect
RemoteConnect R2.4 added support for SCADAPack470
RemoteConnect R2.4.1 supports Realflo flow computer 7.01 (47x controller only) and contains firmware 9.4.2 (supported by Geo SCADA 2020)
RemoteConnect R2.7.2 supports Realflo flow computer 7.10.1 and contains firmware 9.7.2
RemoteConnect R2.7.4 supports Realflo flow computer 7.11.1 and contains firmware 9.7.4 (supported by Geo SCADA 2021 and Geo SCADA 2022)
Unlike the Realflo software that will connect to an x70 controller and read out all values from the flow computer, Geo SCADA requires users to create 'Reaflo' analog input points' which map to different flow computer register types (I.E. Input, Flow Calculation, Hourly History, Daily History, etc).