Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What size ATS48 units require customer-supplied lugs for power connections?
Issue:
Altistart 48 lug kits for power connectors

Product Line:
Altistart 48

Environment:
All

Cause:
N/A

Resolution:
The following need to have customer-supplied lugs on the Power Terminals:
ATS48C14Y ATS48C17Y  ATS48C21Y  ATS48C25Y    ATS48C32Y    ATS48C41Y   ATS48C48Y  ATS48C59Y  ATS48C66Y    ATS48C79Y  ATS48M10Y  ATS48M12Y
These units also require customer-supplied ground lugs.

This is an advantage to customers because they can choose lugs to match the wire size that they're using.