Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is the LH4N still available?
Issue:
LH4N availability

Product Line:
LH4N

Environment:
All models and all serial numbers

Cause:
Customer was looking for purchasing the LH4N112RT7.

Resolution:
No, the LH4N soft starter is obsolete. Please replace with the appropriate ATS01 or ATS22 soft starter. Consider application needs and features of currently-offered products.