Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can an AC drive be used on a 2-speed motor?
Issue:
Wanting to use an AC drive on a 2-speed motor.

Product Line:
Altivar drives

Environment:
All

Cause:
N/A

Resolution:
Yes.
The motor should be connected to the drive with the high speed windings. It is not necessary to use the low speed windings when connected to an AC drive.
It is important to consider the motor full load amp rating when selecting the appropriate drive for the application. The high speed winding is likely the higher rating on the motor nameplate.