Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the difference between the 9080 MH10 and MHA10 end clamps?

Issue
Customer would like to know the difference between the 9080 MH10 and MHA10 end clamps.

Product Line
Terminal Blocks

Environment
All Products

Cause
Product features and selection

Resolution
The MH10 was for DIN 1 and DIN 3 track and is now obsolete.

The MHA10 is DIN 3 only.


CTA-ID : 2014767

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre