Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are the ATS48 soft starters available in a NEMA 3R enclosure rating?
Issue :
Looking for an ATS48 installed inside a NEMA 3R enclosure.

Product Line :
Enclosed 48

Environment :
All

Cause :
Enclosures for the ATS48

Resolution :
Yes. Nema 3R is available in the Enclosed ATS48 packages.
See the attached document.


Schneider Electric Saudi Arabia

Attachment(s)
8800BR0402.pdf [497.89 KB]