Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the maximum UL/CSA AC voltage rating of the LC1D power contacts ?
Issue:
Identifying maximum voltage of an LC1D contactor

Product Line:
TeSys D Contactors

Environment:
Contactors and Starters IEC

Resolution:
IThe maximum voltage per UL and CSA is 600VAC.