Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Do the NEMA 4X stainless steel enclosed combination starters include hubs?
Issue:
Hubs  from Type 4/4X (stainless steel) Sizes 0 thru 0 Enclosures.

Product Line:
Class 8538 and 8539 NEMA Contactors and Starters

Environment:
North American Products

Resolution:
Yes, combination starters in NEMA 4X stainless steel enclosures include two power cable hubs and one control cable conduit hub.