Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why do the drawings in the ATS48 Installation Guide show 2 fuses on CL1,CL2 terminals?
Issue:
Drawings in the ATS48 Installation Guide show 2 fuses on CL1,CL2

Product Line:
ATS48

Environment:
All

Cause:
ATS48 fuse on the CL1 and CL2 terminals

Resolution:
It is not necessary to have two fuses. Only one fuse is needed. Please refer to attached Catalog for updated drawings.

Schneider Electric Saudi Arabia

Attachment(s)
ATS48 Catalog October 2014.pdf [3.79 MB]