Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to convert 8501XO normally open contacts to normally closed in the field?
Issue:
8501XO conversion

Product Line:
Industrial Relays

Environment:
Type X

Cause:
N/A

Resolution:
Remove the top plate and/or adder deck and pull out the contact cartridge then turn it over.  Put the cartridge back into the cavity and install the cover/adder deck .

Green indication through the window indicates a N.O. contact and and yellow indicates N.C. contact