Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is the temperature sensor used in the Altistart 48 soft starter a PTC or a NTC sensor?
Issue:
ATS48 temperature sensor

Product Line:
ATS48

Environment:
All models

Resolution:
The ATS48D17Y, ATS48D22Y, ATS48D32Y, ATS48D38Y, ATS48D47Y, ATS48D62Y, ATS48D75Y, ATS48D88Y, ATS48C11Y, ATS48C14Y, ATS48C17Y, ATS48C21Y, ATS48C25Y and ATS48C32Y use a Positive Temperature Coefficient (PTC) sensor.

The ATS48C41Y, ATS48C48Y, ATS48C59Y, ATS48C66Y, ATS48C79Y, ATS48M10Y and ATS48M12Y use a Negative Temperature Coefficient (NTC) sensor.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre