Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for an electrical interlock for 9422 disconnect switch?
Issue:
9422 auxiliary contact

Product Line:
Operating Mechanisms and Disconnect Switches

Environment:
Class 9422 Flange Mounted and Cable Operated

Resolution:
The electrical interlock for a 9422TC1, 9422TC2, or 9422TC3 is 9999R45 for single pole, double throw or you may use a 9999R46 for double pole, double throw.
See table for the rest:

electrical interlocks