Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the dimensions of the TVS2EMA12A enclosure?

Issue:
What are the dimensions of the TVS2EMA12A enclosure?

Product Line:
TVSS Units

Environment:
Maintenance

Cause:
Replacement

Resolution:

The enclosure dimensions are 14 inches in height, 12.44 inches in width, and 6 inches in depth

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre