Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it ok to use an ATS48 with a Corner Grounded Delta, Ungrounded Delta, or Open Delta system?

Article available in these languages: Spanish

Issue:
Will an ATS48 run with a Corner Grounded Delta, Ungrounded Delta, or Open Delta system

Product Line:
ATS48

Environment:
Corner Grounded, Ungrounded Delta, Open Delta system

Cause:
n/a

Resolution:
It is ok to use Corner Grounded Delta with an ATS48 as long as the voltage is balanced phase to phase.
However, some problems may occur on Ungrounded systems. One or more phases may have a high voltage with respect to ground and may cause measurement irregularities that can affect the operation of the soft starter.
The Open Delta may be a problem because the voltage may not be balanced when loaded. This may cause phase fault problems.




CTA-ID : 2023862