Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What relay should be used to provide two wire control for the Class 8903 Type PB lighting contactor?
Issue:
Two wire control relay for the Class 8903 Type PB lighting contactor

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
NEMA Lighting Contactors

Cause:
Two wire control relay needed

Resolution:
Use any 2 pole relay with a Normally Open and Normally Closed contact, such as
CA2SK11**
8501XO11V**

Complete the part number by adding the appropriate voltage code.  i.e 8501XO11V02 for 120VAC, or CA2SK11G7 for 120VAC.