Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Who supports the Altivar 78 AC drive?

Issue:
Support for Altivar 78 drives

Product Line:
Altivar ATV78

Environment:
All

Cause:
Technical support on the ATV78 drives.

Resolution:
These products are not commercialized in the USA.
They are commercialized in Canada. Call 1-800-565-6699