Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the difference between HC-DB9 and HC-B I-Line boxes?

Issue:
Differences between HC-DB9 and HC-B I-line boxes

Product Line:
Panelboards

Resolution:
The HC-DB9 box is a 9.5" deep box for vertically mounting a Powerpact main breaker. HC-B is an 8.25" deep box for older, pre-Powerpact main breakers.

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: