Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the analog output of the ATV61 or ATV71 be set up as 0-10 VDC instead of 4-20 mA?
Issue:
Needs to set up a analog output of the ATV61 or ATV71 drive, to be set up as 0-10 VDC instead of 4-20 mA.

Product Line:
ATV61 and ATV71

Environment:
All

Cause:
NA

Resolution:
Yes.
Go to the Input/Output menu (1.5) and set AO1 type to voltage (0-10v range). Set AO1 assignment to the proper setting. The minimum and maxim range can also be adjusted inside the 0-10 V or 4-20  mA ranges.