Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the line dip ride through time for the ATV61 and ATV71 drives?

Issue:
What is the line dip ride through time for the ATV61 and ATV71 drives?

Product Line:
Altivar 61 and Altivar 71

Environment:
All

Cause:
Need to know how long the drive will 'ride through' a dip in line power

Resolution:

Maximum running time (without fault) at Under Voltage with Nominal Torque is:

1. 1000 msec. with a voltage 70% of nominal voltage
2. 500msec. with a voltage 40% of nominal voltage