Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can you get an external keypad on a NEMA 3R E-FLEX drive?
Issue:
External keypad option for E-Flex Nema 3R drive

Product Line:
Altivar Machines

Environment:
NEMA 3R only E-Flex drives

Cause:
Needs to order an NEMA 3R -E-Flex drive with a remote keypad display mounted on the door.

Resolution:
The E-Flex drive is obsolete. External keypad was not available on the E-Flex. The replacement ATV660 drive also does not have an option for external keypad on Nema 3R, as they are not UV protected.

Schneider Electric Saudi Arabia

Attachment(s)
30072-454-01.pdf [6.36 MB]
E-Flex_30072-451-51.D.pdf [5.87 MB]