How can we help you today?

What is the largest branch breaker that mounts on the NQOD bus?

Issue:
Largest branch breaker that can be mounted on the NQOD bus

Product Line:
NQOD Panelboard

Environment:
Products sold and used in the United States

Cause:
Installation / Setup

Resolution:
The largest branch breaker for an NQOD panel is 150 amps using the QOB-VH frame. Use the following:
For 2 pole, order QOB2150VH which uses 4 pole spaces
For 3 pole, order QOB3150VH Which uses 6 pole spaces


CTA-ID : 2049573

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre