Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is Ethernet communication available on ATS48 or ATS22 solid state softstarters?
Issue:
Needs Ethernet communication  on the ATS48 or ATS22 solid state softstarters

Product Line:
ATS22, ATS48

Environment:
All

Cause:
NA

Resolution:
The ATS22 and ATS48 only support Modbus communication protocol.
Use a Gateway for Modbus - Ethernet IP conversion.
Consider the EGX150 - Link150 Ethernet Gateway or a device from a 3rd party such as ProSoft or AnyBus.
Please be aware that you cannot do I/O scanning on the ATS48 or the ATS22 soft starter.