Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What does the T indicate in the LC1DT contactor catalog number?
Issue:
LC1DT catalog numbers

Product Line:
IEC Contactors and Starter

Environment:
Tesys D line Contactors

Resolution:
The T indicates that the device is a 4 poles with all normally open poles.  4 pole units only have resistive (AC-1) power contact ratings.