Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to order a 300 amp MCC feeder bucket for Model 5 or 6?

Issue:
Order a 300 amp MCC feeder bucket for Model 5 or 6

Product Line:
Motor Control Centers.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
Yes. A 300A circuit breaker feeder bucket is available in a 24`` branch unit. There is also the posibility to have a 300A feeder bucket with the "High Density Branch Feeder Selection" in a 6" bucket. Note this would have to be worked up on the SE Advantage Product Selector.