How can we help you today?

Are alternative lugs available for an HVMB305200 Minibreak Medium voltage switch?

Issue:
Alternative lugs available for an HVMB305200 minibreak switch

Product Line:
HVL Mini break

Environment:
Installation

Cause:
Alternate wire size

Resolution:
No. There are no alternative lugs available for the compact Mini break switches.
This is due to the lack of wire bending space available with the need to accomodate larger wire or more conductors.

Set screw cable lugs for #14 solid—2/0 stranded aluminum or copper cable are provided for two line and one load connections

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre