Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the replacement for the Flex58 Drives?

Issue:
Flex58 drive replacement.

Product Line:
Flex58, Econoflex

Environment:
All

Cause:
Flex58 drive has failed and needs to be replaced.

Resolution:
Flex58 is an Open Chassis style drive and when mounted inside of an EconoFlex, the heat sink and the fans stick out the back of the enclosure. There is no retrofit kit available to install an ATV630 in place of the Flex58. In most cases, the customer can return the Flex58 drive back to the repair depot for repair or customer can replace the entire EconoFlex with an ATV660 or an S-Flex package unit. If the drive is inside an MCC, then contact a local distributor or field office with the FO# for a replacement bucket