How can we help you today?

For Cartridge Fuses, What is the difference between the two types (aM and gG) ?

- The aM Cartridge fuses are used for the short circuit of equipments with high current peaks
- The gG Cartridge fuses are used for protection of circuits without significant current peaks at starting.

Both types can be with ot without strikers